JPEG Color Compression Using User Library Elements

Brief Description

Files:

\examples\Processing\Compression\JPEG\mE5-MA-VCL\JPEG_DualBaseAreaBayer.vad
\examples\Processing\Compression\JPEG\mE5-MA-VCL\JPEG_SingleFullAreaBayer.vad
\examples\Processing\Compression\JPEG\mE5-MA-VCX-QP\JPEG_SingleCXP6x4AreaBayer.vad
\examples\Processing\Compression\JPEG\mE5-MA-VCX-QP\JPEG_DualCXP6x2AreaBayer.vad
\examples\Processing\Compression\JPEG\mE5-MA-VCX-QP\JPEG_TripleCXP6x1AreaBayer.vad
\examples\Processing\Compression\JPEG\iF-CXP12-Q\JPEG_CXP12Bayer.vad
\examples\Processing\Compression\JPEG\iF-CXP12-P\JPEG_CXP12Bayer.vad

\examples\Processing\Compression\JPEG\SDK\ \examples\Processing\Compression\JPEG\PyPylon\

Platforms:

mE5-MA-VCL
mE5-MA-VCX-QP
iF-CXP12-Q
iF-CXP12-P

Short Description

Simple examples which show the usage of the multiple library elements (JPEG_Encoder_Color_300MPs_VCL, JPEG_Encoder_Color_850MPs_VCL, JPEG_Encoder_Color_600MPs_VCX, JPEG_Encoder_Color_800MPs_VCX and JPEG_Encoder_Color_2500MPs_VCX) of the user library JPEG_Color and of library elements (JPEG_Encoder_Color_iF and JPEG_Encoder_Color_iF_Penta) of the user library imaFlex_CXP12_Tools_Advanced.

In these VisualApplets examples we show the usage of the library elements JPEG_Encoder_Color_300MPs_VCL, JPEG_Encoder_Color_850MPs_VCL and JPEG_Encoder_Color_2500MPs_VCX of the user library JPEG_Color for the compression of color images for mE5-MA-VCL and mE5-MA-VCX-QP platform for various link configurations and input bandwidths. In addition we present examples which show how to use the library elements JPEG_Encoder_Color_iF and JPEG_Encoder_Color_iF_Penta of the user library imaFlex_CXP12_Tools_Advanced for the iF-CXP12-Q and iF-CXP12-P platforms.

For usage of the applets for the platforms imaFlex Quad and imaFlex Penta, a C++ based Framegrabber SDK application as well as a Python based PyPylon script are available. Both applications demonstrate the acquisition and decompression of the JPEG stream. The source code files can be found in the directories listed above.